AXIS#.SAFE.ABSOLUTEPOSVALID

Description

Indicates if the absolute position retrieved from the safe encoder by the safety system is valid or not. It is dependent on whether the read position matches the position stored by the safety system. If it is not valid, a safe homing is required. Absolute position is only requested by functions like SLP. Functions like SLS do not need a valid absolute position.

Value

Description

0

Not valid

1

Valid

Context

For safe encoder details refer to Motor feedback requirements.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read Only

Units

N/A

Range

0, 1

Default Value

0 (Not valid)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.ABSOLUTEPOSVALID

2064h

00h

Unsigned8

-

-

Read only

Yes

AXIS2.SAFE.ABSOLUTEPOSVALID

2164h

00h

Unsigned8

-

-

Read only

Yes